This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-050047: TIDA-050047

Part Number: TIDA-050047
Other Parts Discussed in Thread: TPS25751, BQ25798, BQ25731, BQ25713

Tool/software:

We are planning to design the Power Bank with below configurations.

Connector type (Input side) 

USB Type-C  port 

Input voltage 

5V / 9V 

Input current 

3A / 2A 

Connector type (Output side) 

USB Type-C port  x1, USB-A port  x2 

Output voltage 

USB Type-C is 5V / 9V 

USB-A is 5V 

Output current 

Total 32 W - USB Type-C is 3 A/2.22 A 

USB-A is 2.4 A 

Battery type 

Rechargeable lithium-ion battery 

Battery capacity 

3.6V, 15000 mAh 

Charging time 

Approx. 3 hours 35 minutes  

Request you to please suggest suitable ICs for the same.