Other Parts Discussed in Thread: TPS7H5001-SP
Tool/software:
Hi,
I was running into some trouble while trying to simulate a converter design using the TPS7H5005-SEP transient model in PSPICE. When I use a heavier load of 0.125 Ohms at 5V (40A) my output voltage seems to settle at a little over 3V when the desired value is 5V. When I lighten the load a little and have my load resistance 0.5 Ohms (10A) the transient model works fine and has a steady state output voltage of 5V. I was hoping to possibly get some insight as to if this is something to do with my control loop using the TPS7H5005-SEP model of if there is some other error in my design. I also attached my design files below.
Thanks