This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-00589: Mismatching inductor part with value in schematic

Part Number: TIDA-00589
Other Parts Discussed in Thread: BQ25895

Tool/software:

Hi,

I was taking a look at the reference design for the BQ25895 and the schematic shows a 2.2uH inductor but lists part number IHLP2020BZER1R0M11 in the BOM which is very clearly a 1uH inductor. The description clearly states "inductor, Shielded Drum Core, Powdered Iron, 2.2uH, 8A, 0.018 ohm, SMD" however even looking at the 2.2uH variant of the same inductor series, that is only rated for 5.45A much lower than the 8A written. I can only imagine it was meant to be this part: IHLP2525CZER2R2M01 which is a 2.2uH inductor with 8A saturation however it is a slightly larger package than the one listed. Would this inductor work fine? If not what is the correct recommended part number? 

Thanks!