This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PMP40183: battery charger.

Part Number: PMP40183
Other Parts Discussed in Thread: PMP41163, PMP41117

Tool/software:

Please suggest us one simple battery charger for below specifications

  • Output voltage: 9V
  • Maximum current: 3A

With CCCV concept for lithium ion batteries.

I have searched for PMP40183.and TIDA-1582, Is it suitable for my application?

No need  USB-C connector.

There should be two output wires for positive and negative are sufficient.