Hello Akshay,
The stuff should be enough. I try to verify the model by TI's LM2841Y Pspice Average Model
http://www.ti.com/litv/zip/snvm303
The output voltage of original model is 3.3V. In our case, Input voltage is 12V ,output voltage is 3.0V. So we change the feedback resistor R1 from 3.32K to 2.94K. The simulation result of VOUT become very small. For R1=3.32K, it is about 40dB. What is wrong? Can the working condition of Pspice model be changed ?
regards,
Jerry