I'm wondering the the CSD1850x family NexFET's are slated for TINA-TI model conversion any time soon. I noticed that quite a few of the lower voltage CSD FET's have been converted, but all of the >25V parts are encrypted P-SPICE only for models (for which I don't have access to a compatible simulation tool). The FET will be used with LM3150 for an 8-32V input, 5V output supply. I have done some simulation with WeBench, but I need to do a more detailed transient load analysis. Thanks.
- Sean Byrne