Hello,
i've used the Webench Designer to generate an DC-DC converter with input voltage 8-26V and an output volatage 3.3V with 3000 mA. I used the LM20323 IC.
Error:
In the schematic, ENABLE and VIN are connected, but the absolute maximum rating for the ENABLE-PIN is 6V. We build the DC-DC converter with connected ENALBE and VIN PINS and the LM20323 was destroyed.