Hi,all
I am planning to use LP38513-ADJ for conversions from 2.5V rail to 1.9V.The current needed is 2A. In the datasheet the maximum output current is 3A,but when i evaluate this LDO by WEBENCH,the maximum output current is only 1.4A,Is this right?
I am looking forward your reply.
Thanks.