I'm using the REG113_33 in a battery backup application and need to generate some simulations using MicroCap9. No .lib or .olb for this part is available in MicroCap but I can generate them by using Orcad Capture 14 if I can only get hold of the IC circuit. Does this circuit exist or am I stuck here? The REG113 spec sheet gives very limited information. I have been using the LT1763_33 for preliminary simulations but need the real McCoy from Texas Instruments.
Any help will be much appreciated.
Johann Scheepers