Dear support member,
I have two questions:
- In the datasheet TPS54614 in the section APPLICATION INFORMATION shows a typical TPS54614 application (for parameters Vin: 3V – 6V; Vout: 1.8V). The input filter is a 220-uF POSCAP capacitor. A 10-uF ceramic capacitor for the TPS54614 is required. But in the scheme in WEBENCH Designer (for parameters Vin: 3V – 6V; Vout: 1.8V; Iout: 6A; Ambient Temp: 300C) the input filter is a 47.0-uF. Why the input filter is different?
- Why the TPS54614 scheme (WEBENCH) no Sim Export button?
Regards,
Liudmila Selianova