Hi,
I'm trying to understand about the "Shunt Amplifier 12V" TINA example (Appendix 1). When I'm doing "Analysis-> DC Analysis-> DC Transfer characteristic" I'm getting a graph input current (A) Vs Output Voltage (Appendix 2). According to the graph, in 1A I should get 2V in the output. When I'm doing "Analysis-> Transient" I Get that in 1A the output is 1.19V (As it should according to theoretical calculation). Why the result are not the same?
In addition (and less important from the previous question), in the Transient Analysis, when the input load is 0A I get 1.2V, why is that? (Theoretical calculation showed a different result)
Thank A lot,
Idan Ozana