Other Parts Discussed in Thread: OPA860, TINA-TI, OPA615, LMV7219
I just searched for a voltage controlled current source IC, with wide bandwidth above 50MHz, high adjustable trans-conductance and wide linear range. By comparison, I think OPA860 maybe work. (Actually, I am worried of my searching method, and maybe there are other better VCCS chips.) However, the datasheet is not clear enough.
(1) For the typical connection, the load is resistance. In my application, the load will be the capacitance.Therefore, I am worried whether or not it can still work linearly.
(2) The graph of the relationship between input voltage and output current is only within the range of from -70mV to 70mV, and has no idea of the relationship above this range. Therefore, will it be still linearly beyond this input voltage range? Actually, maybe I hope it can be linear from -200mV to 200mV.
(3) In my application, I may need use this chip in parallel. Will it have some imbalance problems during this application? And what kind of problems? Generally, how to avoid it?
I am looking forward to some reply and answers. Thanks a lot.
Lucy