This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA683 Saturation in Simulation

Other Parts Discussed in Thread: OPA683, OPA684

Hi E2E,

I have a customer who's testing the OPA683 in TINA with the following setup:

  • +V rail = 5V
  • - V rail = GND
  • + input = Sine wave, 200kHz, 200mVpp, 2.5VDC offset
  • Gain of 200
  • Disable is tied to 5V

He is expecting to see saturation but instead sees a 1.89VDC output.

The op amp should saturate with these conditions.  Would the simulation model saturate with these conditions?  Is the model trustworthy in this setup?

Thanks,

-Sam