Other Parts Discussed in Thread: LM5160, LM5017, TIDA-00661
I have an application that will be very close to TIDA-00550, except for two changes:
- Input voltage range is 12-36VDC
- I need to supply more power than is available through the transformer.
I was thinking of using the LM5160 instead of the LM5017, and use the DC-DC converter from TIDA-00661. Are there any issues with redesigning this to accept 12-36VDC?
Thanks,
Caleb