Part Number: OPA627-DIE
Tool/software: TINA-TI or Spice Models
Hi,
I have simulated the attached circuit (OPA627 in inverting mode), and simulation result shows the output noise of 61 nV/rt(Hz) at 10KHz. By hand calculation, I found 64.72 nV/rt(Hz) at 10KHz without considering OPA627 device/model input capacitance of 15pF (differential i/p cap. + CM i/p Cap from datasheet). Now, for this configuration, if I take into account OPA627 device/model input capacitance of 15pF in addition with two external capacitors of the given circuit, my hand calculation shows 68.4 nV/rt(Hz) at 10KHz exhibiting significant difference from previously estimated hand calculation of 64.72 nV/rt(Hz) at 10KHz.
Now my question is:
1. Why does the hand calculation of 64.72 nV/rt(Hz) at 10KHz show the good agreement with the simulation result of 61 nV/rt(Hz) at 10KHz, even though OPA627 device/model input capacitance of 15pF (differential i/p cap. + CM i/p Cap) is disregarded in the calculation?
Kind regards
Jubayer