This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PMP10375: purpose of modified rectifier section / voltage doubler

Part Number: PMP10375
Other Parts Discussed in Thread: PMP10283, PMP9739

Hello Team,

We notice that PMP10375 doesn't use D1 as a normal full bridge rectifier, but it uses an arrangement to place output of two half bridges on top of each other.

What is the purpose of such arrangement? Does it help to improve any design parameter?

Kindly help with your inputs.

Regards,

Mahendra.

  • Hi Mahendra,

    Yes, I use D1 with two series connected bulk capacitors to form a voltage doubler. By doing so, I'm able to have much lower transformer primary current when compare to a converter with a full wave rectifier. With the lower transformer current, I was able to use smaller magnetics and boost efficiency. Here are two similar designs with and without voltage doubler : PMP9739 and PMP10283. You can observe the difference between efficiency and magnetic sizes.

    Regards,
    Sheng-Yang Yu