Other Parts Discussed in Thread: LMX2581, DS125DF1610
Hello,
I hope to find the answer here.
The onboard DS125DF1610 can lock to any frequency in the 9.8- to 12.5-Gbps range or any divide-by-2, divide-by- 4, or divide-by-8 sub-multiples of this range using as input clock either the onboad LMX2581 frequency synthesizer or an external reference clock. Is there a possibility to generate a 8Gbps ? Right now I don't see this option with none of the 3 different pin-compatible retimers.
Thanks in advance!