Other Parts Discussed in Thread: TINA-TI,
Tool/software: TINA-TI or Spice Models
Hi,
I imported TPS62125 model from WeBench into TINA-TI. When I simulate the model with component values as described in slva514b (5V Vin and expected -5V Vout), I get Vout to go past -7.1V with load of 61 ohms.
Expected output is -5V. The output also seems to be highly dependent on load resistor.
Is the simulation model accurate ? Or, is my setup incorrect?
I tried different values of Vin, R1, R2, etc but I always saw Vout much higher than expected.
I saw in another thread that inverting buck-boost topology is not supported in the SPICE models. Is this true?
Thanks,
Satish