I am using the LM53603-Q1 voltage regulator chip with a fixed output voltage of 3.3V and 2.2A max output current. The part works great with an input voltage of 25V but I need it to work down to about 4.5V. The datasheet says it should work with an input voltage down to 3.5V. Also Webench gives an error when trying to simulate with a 4.5V input voltage. Can anybody explain the discrepancy between the datasheet and Webench?
Thanks,
Kevin