This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-00913: TIDA-00913 / GaN , feeadback option,pwm ,fall time <=20nS

Part Number: TIDA-00913
Other Parts Discussed in Thread: LMG5200
 

 

  What GaN evaluation boards/power module  have feeadback option  ?

 

Is possible to control/adjust   frequencies  to  42.8 KHz, 21.4 KHz and 10.7 KHz  ?

 

pulse with 2.5%,5%, 10%  is possible    ? fall time     <=20nS?

 

 

Best regards ,

 

  • Hello Guiseppe,
    though the launchpad you will be able to adjust both the frequency and pulse width.

    Your minimum pulse is dictated by the resolution available at the different frequencies.

    You can refer to the guide for PWM for the TSM320F2806 (page 9):
    www.ti.com/.../sprug02b.pdf

    Regarding the slew rate, this cannot be externally adjusted as it is determined inside the LMG5200 module.

    I hope this helps answering your questions.

    Thank you and best regards,
    Alberto