Tool/software: WEBENCH® Design Tools
hi,
if we are using the component TPS54040 we can to use the TPS57140 inside the TPS54040
thankyou
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: WEBENCH® Design Tools
hi,
if we are using the component TPS54040 we can to use the TPS57140 inside the TPS54040
thankyou
Hello Rosa,
I would not advise you do so, the TPS57140 is a 1.5A device and the TPS54040 is a 0.5A device, the current limit levels are much higher in the TPS57140 device you wish to use. I suggest using webench for the TPS57140 inputting your requirements for the right components to meet your needs.
Hope this helps?
David.