Other Parts Discussed in Thread: SN74LVC2G32
Hello
I was reviewing the schematic of the TIDA-01487 reference desing and I noticed the SN74LVC32APW (U1) is being supplied with an 5V supply, while the datasheet clearly states the operating voltage must be between 1.65V and 3.6V. The maximum voltage is 6.5V but in my opinion it is used outside of the specifications.
Can the SN74LVC32APW be supplied with an 5V supply without problems or is the reference design wrong and should I test it with an 5V alternative?
Best Regards
M. Valentijn