This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-00626: importance of LED D1 when will the LED glow or blink

Part Number: TIDA-00626
Other Parts Discussed in Thread: LMX2592,

Respected,

i have been working on reference design of TIDA-00626. It have a LED d1 connected to MUXout pin of LMX2592 by 330 ohm resistor. i want to know that when will the led glow and what indication will led give

  • Hi Pratik,

    MUXout pin can be configured as PLL lock detect indicator or SDO read back operation. LED D1 is connected to MUXout pin for PLL lock detect indication, when MUXOUT_SEL = 1 and LD_EN = 1 configured. When LMX2592 PLL is locked, LED D1 will glow.

    For more details see page 17 in LMX2592 datasheet for lock detect operation.

    Thanks!

    Regards,
    Ajeet Pal