Other Parts Discussed in Thread: USB2ANY, LMX2592, , LMX2592EVM
respected,
i have developed the reference design of TIDA-00626. but i am not able to program the LMX2592 IC using USB2ANY. i made a thread on LMX2592 they addresed me on working of LMX2592 but were unable to address the debugging procedure for TIDA-00626. i am unable to power down the device using TICS-pro software and at the same i am unable to lock the VCO . i would first like to say you what testing i have done.
1. the power supply section of TIDA-00626 is working perfectly and giving me all appropriate voltages.
2. My USB2ANY is also working properly tested it by using TICS-PRO software and pressing the II=identify button and USB2ANY green LED blinks.
3. connector for USB2ANY is placed properly.
4. i have disconnected r15 and r13 from the board as i prefer using the on board crystal oscillator of 100 MHz.
5. the power consumption of board is arround 400-450 mA but the specified power consumption is of 750 mA is this fine.
5. as specified in LMX2592 forum the said me trie to power down the device and eventually your current consumption will reduce and the voltage at OSCin pin will drop to 0(power down) and is 1.6v(powered up). but i am not able to power down the device.
please help me to debug this fault of USB2ANY connection so that i can get my signal generator working. please mention steps to debug the circuit.
kindly address us as soon as possible any help will be highly appreciated.