Hello,
I am using the coldchain code to work with TIDA 00524. I am getting sensors readings every polling interval, which is the minimum is 1 minute. However, I want to add extra interrupt to make the measurements happen every time I am reading out the data logger as long it is in start case. For example, if the data-logger collecting humidity and temperature sensors every 5 min, I want to add another interrupt to add extra real time measurement once I scan the data logger with the reader. I tried to play with p2.5 interrupt and added extra flag in there, but It didn't work for me.
My question: Is it possible to get real time measurements while scanning with keeping the polling interval pattern. and what is the best way to do it
your help will be appreciated
Thank you