Other Parts Discussed in Thread: CSD18502Q5B, , CSD18502KCS
I am working of your Solar charge controller reference design TIDA-00120. I have designed the PCB, mount the components and program the MCU according to your site instructions. All thing are work properly but when i have test it on highest capacity of charge controller of 19.5A at 12.5v on battery the Q6 mosfet CSD18502Q5B than present for battery reverse protection is heats at 125 degree C when environmental temp. is 28 degree C. How can i reduce the temp. of this mosfet.
I have also use it on 15A configuration but there is heating around 95 degree C, which is not match the thermal calculation of this mosfet.