This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-00555: power supply of TIDA-00555

Part Number: TIDA-00555
Other Parts Discussed in Thread: TIDA-00810, TIDA-00835, TIDA-00080, TIDA-00834

Dear Experts,

I am a postgraduate student from Hong Kong. I am quite confused when I tried to realize the reference design TIDA-00555. I started with the power supply part, and after finishing the following as shown in figures, I can not get the voltage as shown in the schematic,+6V and -6V. Instead, the voltage across C77, C80 is about 19V, and C73, C75 with -19V.  However, the voltage across D24 is correct +5V, thus D9 works well. Meanwhile, the voltage across D22 is -1.5V, instead of -5V, as a result, D11 does not work. 

I have checked if there is something wrong with about the soldering, and tried other three PCBs, but can not find anything. So, I am wondering if there is something I need to be noticed. I would be appreciated any replies!