Other Parts Discussed in Thread: CC1310, TIDC-01002, CC1150, CC1020
Hello,
I want to replace RS-485 connection with wireless one and to increase a distance.
Now up to 10 temperature sensors are connected to PC with RS-485 as daisy chain.
These sensors are placed across the line of sight and send results on PC request.
In a new project I want to avoid the cable connection and increase a distance up to 2-3 km between the PC and the last sensor in the chain (possibly up to 16km distance would be needed in future).
The PC should collect results in real time every 1-2 seconds (the sensor's result consists of 3 bytes).
Delays in the results receiving are not permitted, my application should get them directly - not from a cloud or some server.
(Or if the delay is a few seconds, it should be known and stable - but this is worse).
Is it possible to use TIDA-00484 as node and may be CC1310 wireless MCU LaunchPad™ development kit, connected to PC, to provide wireless connection on 2km distance and to get data with minimal delay (<1s)?
If this technology is not correspond to a project, whould You advice me another ST technology?
Best regards,
Vadim