This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-00122: UCD 8220 and MSP430 design question

Part Number: TIDA-00122

Dear Sir,

i have a customer that need to convert from DC voltage 12v to AC voltage AC110V_total watts 100w~150w(60 Hz sinewave) inverter application. the reference design about TIDA-00122 can i ask a few questions?

1.do you have a MSP430G2330 source code? for TIDA-00122 reference design.

2.do you have a datasheet for transformers(T1_EI33 12PIN BOBIN)?

3.if changing the input voltage from 12v to 24v i need to change which components or parameters?