Other Parts Discussed in Thread: TIDA-00499,
Hello smart TI ENGINEER
NOW I WANT TO DESIGN A BOARD to collect the voltage of High voltage(10kv~110kv) circuit breaker 。the Collected voltages range from -450V to +250V, or from -65V to +60V。There are four pictures below,the first pic is the digram of the whole frame,the second is the signal of a point which is Affected by VFTO,the third one is the signal of B point which is also Affected by VFTO. THE LAST ONE IS THE signal of A point and B point and c POINT and d POINT AT STEADY STATE. Can you recommend me a similar reference design? or some suggestion on Common treatment of such signals! thank you very much !