Other Parts Discussed in Thread: ISO1050, LM25018, , BQ76930, BQ76940
Dear TI experts,
As is shown in reference design(tida-01093), the supply voltage of iso1050 CAN transceiver is 5V, so LM25018 regulator is needed to offer the voltage.
I wonder if I could use a CAN transceiver whose supply is 3.3V. In this condition,the LM25018 is no longer necessary. the can transceiver is powered by bq76930 or bq76940.
Is this design feasible?Or are there some problems in the design?Why do your experts design the reference design in that way?
I wish your early reply.
Thanks & Best Regards