Other Parts Discussed in Thread: BOOSTXL-TLV8544PIR, CC1310, , CC2650
Hey guys,
I have adopted the TIDA-00489 Firmware by changing the RF settings, using the export function of SmartRF Studio 7. I exchanged the smartRF_Settings files in the project. Since I don't have the actual TIDA-00489 module yet, I wanted to "simulate" the board using a CC1310 launchpad and a BOOSTXL-TLV8544PIR module.
I noticed in the board.c file, that
#include <ti/sysbios/family/arm/cc26xx/PowerCC2650.h>
is included. Thus I thought, that the pin map of CC2650 is equivalent to the one of CC1310. Furthermore, I checked the CC2650 launchpad, which looks very similar to the CC1310 ones (comparing the jumper pin lanes).
Altogether I have two cc1310launchpads and the BOOSTXL device. I want to see if I can make some tests using the sensor + cc1310 on the one hand and on the other hand I'd like to use SmartRF Studio - "Continuos RX" feature to see if it works.
Question:
Can I use the TIDA firmware in this hardware setup, without making changes to the code, especially the PIN-mapping?
I hope you guys can help me getting started. Please notice, that I am more or less a beginner in C/C++ programming, although I have some experience with MATLAB or LabVIEW.
kind regards
Stefan