Other Parts Discussed in Thread: UCC28180
Hi
We have made a proto based on TIDA-00443, In this design the Vsense equals 4.99 V for a output voltage of 391 V.
What shd be the Vsense value in the boost follower mode. I guess it shd be equal to 5 V for a o/p voltage ranging from 290 V to 390 V.
Then only it could maintain a varying o/p voltage for different value of i/p AC
We were just checking the Vsense value by disabling the controller. (Just varying the I/P AC voltage and measuring the o/p voltage and Vsense value)
we noticed that the Vsense was varying ( not constant as we expected) and it was around 4.5 V for a output of 390 V DC. Is this correct ?
What shd be the correct value of Vsense for a o/p voltage of 290 ~ 390 V DC in boost followe r mode ?
Thanks
Lenin.