This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-00361: Is there a drawing for the camera stand?

Part Number: TIDA-00361


The picture of the system has controller, projector and a camera on a stand.

Is there a drawing for the stand?

We are trying to build the evaluation system like for like.

http://www.ti.com/tool/TIDA-00361

Thanks,

Ugnius

  • Hello Ugnius,

    This stand was made in our internal shop and regrettably does not have a drawing.

    It should be simple to manufacture by hand in a shop (as we did for the one shown).

    Make it so the angle the camera is pointing (up/down) with a little adjustment.  The vertical offset is about 8 inches.  It is not super critical.  What is more important is selecting the right lens to get about the same field of view as the projector at the distance of interest.

    Fizix