Other Parts Discussed in Thread: TINA-TI, , TLV3012
Tool/software: TINA-TI or Spice Models
Hello,
We are using TlV3012-Q1 comparator for power level detection. We would like to set power under voltage detection at 11V. Now we want hysteresis of 0.4V. We connected circuit as per datasheet in figure 23. That gives us values 115K and 10K for hysteresis of 0.4V.
Now we want comparator output changes transitions at 11V and 11,4V, simulated circuit in TINA however at 11.4V it does not changes. I have attached TINA file for reference. Can anybody confirms that our circuit is OK or any alteration is required?
sboc082a -W 1.tsctlv3012-q1.pdf
Regards,
Amod