Other Parts Discussed in Thread: DAC38J84
Dear all,
one of my customer is going to replicate in the lab the setup of the TIDA-00996 in order to synchronize 8 DACS. The frequency in place are lower than the capabilities of the DAC3xJ84 (fs about 240MHz, fout in the range between 20MHz and 100MHz).
1. Can the DAC3xJ84 support those low frequencies ? The EVM of the DAC38J84 has some balun at the output (min freq 10MHz), which is the behavior at 20MHz ?
2. Is it possible to trigger the generation of the DATA from a trigger input (also on the master TSW14J56) instead of the GUI ?
thanks,
Domenico