This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools: LM5141 driver was very weak ,IC was hot when input over 18V

Tool/software: WEBENCH® Design Tools

This is my second design LM5141,40V-5.2V DC-DC

I design the EVM refer  to the WENBENCH tool schematic

When input is 40V,output is 5.V 3A,IC and MOS are very hot,about 100℃,

Here are there picture about the high and low MOS driver waves,in different output current。

Blue diagram is high MOS driver

Yellow diagram iS low MOS driver

output is1A

output is 2A

output is3A

See the above there picture,when operate the different output current ,the high MOSFET driver open time almost keep unchanged

Let us see the low MOS diver wave changes in different output current

1A

2A

3A

I am in interrogative ,as usual,when the loading is added,the high driver should gain the duty cycle in the buck circuit,Otherwise  this state  is not my hope, and  why only  the low driver duty cycle was added when the output current  was added 1A  to 3A? 

I have  test  the high MOS Vgs,the wave was very strange

It was seen like not as full work,I gusset if it is the reason why MOSFET was very hot,even the output is only 1A

So my main question is something case the IC and  MOSFET hot,I hope someone can help me to solve this problem?

I am sure that  IC GND is enough,because the IC is not  pover  device

I found main reason was that high MOS driver is very weak when  the input over 20V 

like this pictures:

input is 12V,higt MOS Vgs is normal ,IC and MOS can't be hot

input is 30V,higt MOS Vgs wave is Disorderly,IC and MOS are hot

input is 40V,higt MOS Vgs wave is more in trouble

the driver is very weak,so that the MOS be  hot when load 。this state  I have been understand

But  the IC be hot when input is higt voltage,and the driver wave can't serve MOS switch fully,

So what case the IC can't work in high input voltage?