Other Parts Discussed in Thread: TPS27S100,
What are the benefits of using TPS27S100 (Single-Channel High-Side Switch) in the implementation of safe torque off functionality in Variable Speed Drives?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
What are the benefits of using TPS27S100 (Single-Channel High-Side Switch) in the implementation of safe torque off functionality in Variable Speed Drives?
TIDA-01599 is a TI Reference Design that implements safe torque off functionality in variable speed drives (per IEC61800-5-2).
TPS27S100, which is a Single-Channel High-Side Switch, is used to turn ON/OFF isolated IGBT gate driver supply for implementing safe torque off (STO). It offers the following benefits in this STO implementation:
For additional information about this topic, please refer to section 2.6 "System Design Theory" of the User Guide for TIDA-01599.
You can also download the design files (BOM, Schematic, Gerber) for this reference design from the TIDA-01599 folder.