Other Parts Discussed in Thread: LMX2594,
Hi!
Can you tell me, please, why didn't you cover transmission lines in the TIDA-01021 (those, which are connected with LMX2594) with mask?
Thanks in advance!
Best regards, Vic.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi!
Can you tell me, please, why didn't you cover transmission lines in the TIDA-01021 (those, which are connected with LMX2594) with mask?
Thanks in advance!
Best regards, Vic.
Hi, John! Thanks for the reply!
Maybe Clock & timing would be better.
Best regards,
Vic.
Hi Vic.,
In TIDA-01021 board, LMX2594 output signals can go higher up to 15GHz and to improve the insertion loss & return loss at high frequencies, mask was removed on the high frequency traces from LMX2594.
One can have mask on these traces / transmission lines as recommended by the Fab vendor to minimize the insertion loss at operating frequencies.
Hope it answer your above query.
Thanks!
Regards,
Ajeet Pal