Other Parts Discussed in Thread: ADC12DJ3200EVM, LMK61E2, ADC12DJ3200
In the process of synchronizing two ADC12DJ3200EVM boards and 2 TSW14J57 JESD204B under design TIDA-01021 I have run into a strange issue.
I connected to one of the TSW14J57 boards through the HSDC Pro software as normal and then tried to connect to the other TSW14J57 board on the same computer. After this did not work I noticed that one of the TSW14J57 boards (the 1st board) was malfunctioning. It had improperly powered down, all of the photodiodes were off, the fan had stopped spinning but was jittering in place.
After powering down the TSW14J57 board I was able to restart the board, and connect to it with the HSDC Pro software, however now if I try to load firmware to the board it will shut down.
I am not sure if this is a mechanical issue or a firmware issue and I need help knowing how to proceed with troubleshooting this issue.
Thanks,