Part Number: TIDA-00366
Dear TI Experts:
I think TIDA-00366 is a wonderful design example!
We can find some specifications in the TIDA-00366 document, shown below.
"Reinforced Isolated Inverter Suited for 200-V to 690-V AC Drives Rated up to 10 kW"
"DC bus input voltage: 400 to 1200 V (Table 1)"
"Motor Three-phase 400-V AC induction motor (Table 1)"
In Page 7 of TIDA-00366 document, it mentions that Line-to-line voltage (VLL)=415V AC, which is an important parameter for the following derivation.
Could you kindly show me how to get Line-to-line voltage (VLL)=415V AC? I hope to apply the concept to other designs.
Happy New Year!
Tang Han