Hi!
I want make a similar desing PMP11303 for a 55V output and 6A. I made the design, but if i don´t have output load the voltage is over the 55V (90V) for this reason i want knowing if it's necesarie a outputload for a correct output in PMP11303 desing or it's possible that my desing it´s incorrect. (The schematic it's similar but with other values)
Thanks.