This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-00079: inductor selection

Part Number: TIDA-00079

Can you please provide the dimension of L1,L2,L3 Inductor because the manufacturer is not responding. so I am going for custom design. So can you please help me with details like:

Core name or dimensions:

conductor dia:

the number of turns:

L1 INDUCTOR, 790uH, 30A, 10%, TH
L2, L3 INDUCTOR, CHOKE, COMMON MODE, 2.5 mH, 30 A, TH
  • Hi,

    I hope you are taking about
    L1 = FIXED IND 4.7UH 3.8A 27 MOHM SMD (Part number: VLC6045T-4R7M and Manufacturer: TDK Corporation)
    L2 = FIXED IND 10UH 1.3A 150 MOHM SMD (Part number: 744042100 and Manufacturer: Wurth)
    L3 = FIXED IND 1UH 3A 19 MOHM SMD (Part number: ELL-6RH1R0M and Manufacturer: Panasonic Electronic Components)

    If yes, followings are the dimensions:

    L1 = (6.00mm x 6.00mm x 4.50mm)
    L2 = (4.80mm x 4.80mm x 2.00mm)
    L3 = (6.40mm x 6.00mm x 2.80mm)

    Since the core name and conductor diameter are not mentioned in the inductor datasheets, it would be better to check those details with manufacturer only.

    Kindly let me know if you have further questions.

    Thanks,
    Sharad