Other Parts Discussed in Thread: TINA-TI,
Tool/software: TINA-TI or Spice Models
I'm running a Trial version of PSpice. I downloaded PSpice model and a project example THS4524 PSpice Model (Rev. B). The example with AC simulation works OK, but if I add a pulse voltage source for transient analysis with out even connecting it to the main amplifier circuit even the AC simulation starts failing with the error:
ERROR(ORPSIM-16550): Floating point computation failed during matrix solution. Possible solutions: 1)Ensure that all device parameters are in valid range. 2)Try using .options LIMIT
INTERNAL ERROR -- Overflow, Multiply
ABORTING SIMULATION
Transient analysis fails too.
Do you know if there is an OrCAD example with a PSpice model of THS4524 for transient analysis?
Please, see the whole schematics, I used, below. The only modification from the original one is V8 and R6.
Thank you!