This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-010015: SYN rectification MOSFET selection

Part Number: TIDA-010015
Other Parts Discussed in Thread: CSD19505KCS, UCC24612

Hi ,

I just want to confirm the selection of secondary side sync rectification  MOSFET in TIDA-010015 model. In datasheet it is mentioned that the mosfet should have atleast 7mOhms with respect to  3A rms 14A peak .

For this TIDA-010015 model considering continuous current like 21A the minimum RDson is 4.7mOhms.So the selection of mosfet RDson should have more than 5mohms . But in this design the selected mosfet (CSD19505KCS) RDson is only 2.6mOhms. Can anyone explain the concept here since im using this design for our application want some clarification in the component selection. 

Seems like efficiency trade off for conduction loss. Correct me if im wrong .

What if i use the same mosfet for our design will it be ok ? shall i try parallel mosfet to minimize the heat dissipation ? If im using parallel mosfet do i need reconsider the RDSon parameters and i found related post suggesting not use syn rectification if RDson less than 3mohms. 

Link for the post: https://e2e.ti.com/support/power-management/f/196/t/691605

Please advise

Regards,

Bala