This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/LM3414: LM3414 is not appear Webench selection

Guru 19635 points
Part Number: LM3414

Tool/software: WEBENCH® Design Tools

I trying to simulate LM3414 on Webench below condition.

But LM3414 was not appear selection list and list of "Show why other parts were not found".

Is there any bug on Webench?

Or, what is the reason for LM3414 can't simulate?

------------------------------------

・LED Operating Current: 350mA

・Vforward: 2.6V

・# Series: 6 (= 15.6V)

・# Parallel: 1

・Configure Power Source: DC

・Vin min: 21.6V ~ Vin max: 26.4V

------------------------------------

Best regards,

Satoshi