This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-01442: are DA4_P/M and DB4_P/M signals swapped on the FMC connector?

Part Number: TIDA-01442
Other Parts Discussed in Thread: ADC12DJ3200EVM

DA4 is connected to DP12_M2C

DA5 is connected to DP10_M2C

DA6 is connected to DP8_M2C

DA7 is connected to DP9_M2C

Shouldn't DA4 be connected to DP11_M2C?

DB4 is connected to DP11_M2C

DB5 is connected to DP13_M2C

DB6 is connected to DP14_M2C

DB7 is connected to DB15_M2C

Shouldn't DB4 be connected to DP12_M2C?

Seems DA4 and DB4 are swapped. Has this been fixed in a later revision of the TIDA-01442 board? This is affecting quad pin assignments on our FPGA on the FMC carrier board.

Regards,

Paul Young