Part Number: PMP4925
Hi John, Having resolved the minimum input level; Iz the PMP4925B ,a EValuation Module or only ref designI would hv liked to explore one for UCC2897A ic. Can it be sampled?If yes ,how?pls Guide,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: PMP4925
Hi John, Having resolved the minimum input level; Iz the PMP4925B ,a EValuation Module or only ref designI would hv liked to explore one for UCC2897A ic. Can it be sampled?If yes ,how?pls Guide,
Hi Sonal Singh
Ok, in this case then UCC2897A EVM can be supplied as sample? Is it possible?
Secondly , How much max duty cycle a designer can go in Active clamp? TO be specific is it ok if 65% duty is planned (to reduce size of Trf)?
Is any doc available to calculate the FET & TrF loss?
If so pls provide us
thanks... Dattaray
Hello Dattaray,
You can order the EVM on the link below:
The maximum duty cycle of 70% for UCC2897A is considered as a normal operation, you will be fine there.
The paper below has a very thorough approach on how to calculate the power losses across the transformer: https://www.ti.com/lit/ml/slup126/slup126.pdf
Use this paper to calculate the losses related to the primary FET: http://www.ti.com/lit/an/slyt664/slyt664.pdf
Regards,
Sonal