This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-01028: Missing part numbers in BOM

Part Number: TIDA-01028

I would like to know the part numbers of capacitors used in TIDA-01028 board having the following ratings

(1) 100nF, 50V

(2) 1uF, 16V

(3) 10uF, 25V

  • Deeksha, hello and thank you for your interest in Texas Instruments' Reference Designs. Your query has been forwarded to the design owner for this design on our Industrial Test/Measurement team out of TI-India. You should hear back from him in the next business day. As is the case for most standard passive components, when a manufacturer is not specified, you can select a standard capacitor given you have the necessary component parametrics. Anbu can advise as to the exact manufacturer component used, however, in the meantime, please consider the following based on the parametrics provided in the BOM (all are 10% Tolerance Caps):

    WCAP-CSGP Ceramic Capacitors, 0603, X7R, 50V, 100nF - MFR: Wurth Elektronik, P/N 885012206095
    WCAP-CSGP Ceramic Capacitors, 0603, X7R, 16V, 1uF - MFR: Wurth Elektronik, P/N 885012206052
    WCAP-CSGP Ceramic Capacitors, 1206, X7R, 25V, 10uF - Wurth Elektronik, P/N 885012208069

    Best Regards,
    J. Fullilove
    Reference Design Operations
    Texas Instruments
  • hi Deeksha,

    Thanks for informing MPN is missing ..  I will update BOM in ti.com. let me know if you have any further query.

    Here find the part no of those capacito r.