Other Parts Discussed in Thread: TINA-TI,
Tool/software: TINA-TI or Spice Models
Dear Sir or Madam,
I am doing the operation simulation of TPS22914C with TINA-TI.
The simulation model was created by downloading snvm667.zip on the TI website and using TINA-TI's Pspice netlist import function.
However, the results are not as expected.
Specifically,
-VIN=3.3V
-A divided voltage of VIN is input to the ON pin (0.5VIN=1.65V).
-Looking at the data sheet, the minimum VIH at the ON pin is 1V, and it should turn on without problems if it is 1.65V.
-However, although the voltage of VOUT rises for a moment, it drops immediately.
Please let me know if there is a cause of the behavior of VOUT.
Best regards,